EEO#.LINES

Description

Sets how many lines are output for one revolution of the source feedback. When configured to output CW/CCW or step/dir signals (EEO#.MODE 1 or 2) you will get 4 times this value of pulses per revolution.

Examples

Code

This will set the number of EEO2 lines to 8096.

-->EEO2.LINES 8096

Context

For more information see Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 16777215
Default Value 1024
Data Type Integer
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.